Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Product List
USBSypder08-Slide13

An example application for the Spyder08 Kit is the conversion of a sewing machine controller from an electromechanical to a fully electronic system. Traditionally, sewing machine controllers have employed a pedal to control the motor speed by varying the applied voltage. These types of systems are expensive and energy inefficient. An improved design utilizes an accelerometer as a tilt sensor and a low-end microcontroller for energy efficient PWM motor control.

PTM פורסם ב: