Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Product List
USBSypder08-Slide7

Contrary to traditional in-circuit emulation which requires an external emulator, the Spyder08 uses the target microcontroller to perform in-circuit execution. The Spyder08 tests all of the microcontroller’s peripherals in real life and does not reconstruct or simulate them. This debugging approach ensures that the target microcontroller’s electrical characteristics (including pull-ups, low-voltage operations, and I/O thresholds) are 100% guaranteed.

PTM פורסם ב: