Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Product List
USBSypder08-Slide14

The CodeWarrior Development Studio can be used to create the system firmware to interface with the accelerometer and control the DC motor power stage with a PWM signal. Once the firmware has been developed, the microcontroller can be inserted in to the circuit and fully tested with the in-circuit debugging capabilities of the Spyder08.

PTM פורסם ב: