Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Product List
ben9

Over the Air (OTA) updates make it possible to update RIIoT™ in the field. OTA can save large costs compared to sending out installation staff to upgrade network nodes with bugs that are already installed in the field, and it can also be used to add or modify the local data processing needed for changes in the environment.

PTM פורסם ב: