Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Product List
comm open

A RIIoT™ gateway can be done in many ways. Here are the existing solutions that Radiocrafts has supported up to now; additionally, there are more gateways being added all the time. Radiocrafts supports solutions for customers with specific requirements on the gateway. Radiocrafts can support most gateways, but each case needs to be checked. Radiocrafts should confirm that the gateway works prior to decision; contact Radiocrafts for a quick assessment. Radiocrafts also supports solutions which apply to the customer who wants to make a special design; contact Radiocrafts to ensure that the RIIoT net controller supports the target processor. Consult the GPR datasheet for details on how to interface to the module. The RIIoT gateway dongle is optional to simplify the integration of the GPR module and can be part of the system or the customer can decide integrate to the GPR module as an RF module.

PTM פורסם ב: