Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Product List
tools

There are three tools that are developed for RIIoT™ design. First is the RIIoT development kit, which is orderable from authorized Radiocrafts distributors. It contains three boards with antennas that can be used to set up a simple star network. The three boards allow users to create a network as well as test and debug the network performance and ICI application. Second, the RIIoT SDK, which is downloadable from the Radiocrafts site, contains all tools, scripts, and documentation needed to create ICI applications to configure the SPR modules. Lastly, the RIIoT network dashboard is a tool to monitor the network status.

PTM פורסם ב: