Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Product List
Advantages of Using High EMI Immunity Op Amps-Not Affected by Noise

The advantages of ROHM‘s EMARMOUR™ op amps are explained here. The figures shown are examples of a current detection application, comparing a conventional op amp with ROHM’s EMARMOUR op amp. This circuit amplifies the voltage generated when a current flows through a shunt resistor. In the case of the conventional op amp, the input signal and external noise are amplified. This can cause unexpected malfunctions in the system. However, the EMARMOUR op amp amplifies only the expected signal, ensuring stable operation as it is not affected by external noise.

PTM פורסם ב: