Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Product List
ROHM’s Op Amp Product Roadmap

This slide shows the product roadmap of ROHM’s op amp products. The horizontal axis is the slew rate, and the further the customer goes to the right indicates higher speeds. The vertical axis is the input offset voltage, and the smaller the value means the higher the accuracy. The features and input/output type of each product are indicated. ROHM will continue to expand its lineup by developing products specializing in various characteristics such as higher precision, higher speed, and lower consumption.

PTM פורסם ב: