Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Product List
RF Reed Relays Presentation - Part 2 Slide 16

To match Standex-Meder’s RF reed relay testing results the designer many times will need to add some circuitry in the form of inductance and capacitance at the input and output of the reed relay. This ‘tweaking’ is usually required because the geometries of the PCB and the reed relay will be slightly different. The designer is also matching other components on the PCB nearby the reed relay as well.

PTM פורסם ב: