Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Product List
RF Reed Relays Presentation - Part 2 Slide 2

The characteristic impedance (Z) was already introduced in Standex Electronics’ RF part I, and it will be one of the parameters focused upon while looking at the materials and geometry of the reed relay. For best RF performance the characteristic impedance must be consistent along the entire signal path. This includes the entry and exit points in and out of the reed relay. Most RF circuits today are 50 Ohms (Ω). So, at any given point, at the entry, thru the reed relay, and exiting the relay, the characteristic impedance must be maintained at 50 Ω.

PTM פורסם ב: