Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Product List
RF Reed Relays Presentation - Part 2 Slide 21

The SIL and MS series are in-line single reed relays shown here, the top image, the distance within the SIL relay from A to B is approximately 0.70 inches which is a little shorted than the LP relay. So it should so have better RF characteristics because of the shorter signal path. The MS relay is even better and is only 0.50 inches inside the relay from point A to B, so the RF characteristics will be better still. Note however, the reed relays still have the inputs and outputs going through the PCB on both sides of the relay.

PTM פורסם ב: