Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Product List
RF Reed Relays Presentation - Part 2 Slide 24

As discussed in the first RF discussion, the RF isolation is the ability of the reed relay to isolate the signal when the relay contacts are open. Because of the capacitance that exits across the contacts, some RF signal can ‘leak’ across the open contacts particularly as the designer increases RF frequencies. When one increases the reed switch gap distance, this decreases the capacitance which in turn improves the signal isolation. The gap distance increase is directly related to an increase in the ampere-turns (AT) of the reed switch. This will require a stronger coil requiring more power to operate or close the reed contacts within the relay.

PTM פורסם ב: