Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Product List
RF Reed Relays Presentation - Part 2 Slide 1

Welcome to the Standex Electronics’ RF Reed Relays Presentation – Part 2 product training module. This presentation assumes that users have already gone through the first Standex Electronics’ RF part I presentation. If not, Standex Electronics suggests that users go through Part 1. Understanding the simple physical layout of a reed relay makes it easy to design and test reed relays for RF and fast digital pulse applications. RF is dependent on the physical layout or signal path it takes while going through circuits and the components that make up those circuits. The engineer will show how the physical layout of the reed relay will have a direct bearing on the RF signal’s success going into and out of the reed relay. Coupled with the relay’s physical layout, the materials making up the reed relay are also important.

PTM פורסם ב: