Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Product List
DC-DC Conversion Cookbook Slide 10

As an example of the importance of low quiescent current this slide shows what happens in the real life case of the STM32L. The power supply required from is 1.8 V to 3.6 V, from 1 µA in standby to tens of mA in the run mode. Where there is a problem is with the 1 µA, because that is lower than the quiescent current of many regulators. The power supply will require more power for itself than it is actually delivering to the load. Hence the importance of low Iq regulators or even better regulators whose efficiency is high even at light load, such as the STLQ015 LDO or L6928 switching regulator.

PTM פורסם ב: