Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Product List
DC-DC Conversion Cookbook Slide 2

A voltage regulator, whether it is linear or switching, is a device designed for the basic need to keep a constant output voltage and achieve a certain load and line regulation (that is, to keep the output voltage stable when the output current is changing or when the input voltage is changing). When talking about voltage regulators, these three numbers are always the basic parameters and the primary buying choices.

PTM פורסם ב: