Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Product List
DC-DC Conversion Cookbook Slide 8

The voltage mode is not the only way of closing the loop. In current mode control, in addition to the feedback voltage, there is an inner feedback loop that monitors the current. A current sense amplifier senses the inductor current and converts it to a voltage. This signal is fed to a comparator together with the output of the error amplifier and the slope compensation. Slope compensation is necessary to avoid sub-harmonic oscillations, the details of this go beyond the scope of this presentation. As in the voltage mode, during each cycle, the PWM comparator modulates the power transferred to the load, but this time the inductor peak current is also changed based on the feedback error voltage. This is the principle of a slope compensated, current mode PWM control, which provides stable switching and cycle-by-cycle current limiting for excellent load and line response.

PTM פורסם ב: