Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Product List
DC-DC Conversion Cookbook Slide 11

STLQ015 consumption at zero load (because when supplying to a micro in standby the load is close to zero) is 1 µA as opposed to several tens of µA usually specified for LDOs. This is a suitable device to supply a µC in standby. The trade off for lower power is speed. Low Iq regulators have poor transient response characteristics. When an excellent load transient is highlighted in the list of features, it means the transient response is excellent for a low Iq regulator, not as an absolute. The STLQ015 is designed to achieve a balance between fast transients and low quiescent current. There are competitors’ devices with lower Iq, but the transient response is poor, which is a problem in an application once the micro enters the run mode and the load increases rapidly.

PTM פורסם ב: