Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Product List
Slide17

The low ESR is a feature of the MLCC, but it is so much lower compared to an aluminum electrolytic capacitor that on the contrary, the output voltage of the DC-DC converter becomes unstable and causes oscillations to occur. As shown here in the figure, the DC-DC converter compares the output voltage with the reference voltage, amplifies the error amount with the error amp (error amplifier), and performs negative feedback to achieve a constant and stable direct current voltage. However, signal phase lag occurs due to the inductor (L) and the capacitor (C) of the smoothing circuit. As the phase lag approaches 180°, a positive feedback condition is created, causing it to become unstable and oscillate.

PTM פורסם ב: