Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Product List
Slide22

The ESR Control MLCC series was independently developed by TDK to effectively deal with this issue. This capacitor has a structure similar to the three-terminal pass through type of capacitor. By using combinations of multiple internal electrode patterns, this enables the design of higher ESR values by changing the conductive resistance value within the layered body. This allows for products to have a modified ESR value without changing the capacitance, chip size or the withstanding voltage.

PTM פורסם ב: