Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Product List
Slide19

Previously, electrolytic capacitors and MLCCs where connected in parallel for decoupling in an analog circuit, but with the productization of large-capacitance MLCCs, the replacement of electrolytic capacitors with MLCCs is advancing. In particular, large-capacitance is required to reduce impedance due to the large ESR in an aluminum electrolytic capacitor. However, an MLCC does not need the same capacitance as an aluminum electrolytic capacitor, because low ESR is a feature of the MLCC. The miniaturization and low-profile of the MLCC also achieves a reduction in circuit board space, and the long lifetime and superior reliability are also replacement advantages.

PTM פורסם ב: