Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Product List
Slide26

In summary, TDK offers an abundant lineup of MLCCs for achieving success in the replacement of aluminum and tantalum electrolytic capacitors. TDK also provides an ESR Control MLCC which can control the ESR value in order to inhibit anomalous oscillations and anti-resonance. Please select the right MLCC for the application to improve the reliability of the products. In recent years, the productization of high-capacitance MLCCs of several dozen to over 100 µF has made it possible to replace tantalum and aluminum electrolytic capacitors. The switch to MLCCs in a wide range of consumer and industrial devices is advancing due to the high rated voltage, superior ripple control, long lifetime and high reliability. The weakness of the high-dielectric MLCC is the reduction in capacitance due to temperature or the application of a DC voltage (temperature characteristic, DC bias characteristic). In addition, the extremely low ESR feature can cause anomalous oscillations and anti-resonance to occur, so caution is needed when replacing capacitors.

PTM פורסם ב: