Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Product List
Slide23

The MLCC is a superior capacitor, but it also has weaknesses. The capacitance of an MLCC changes according to the applied voltage. This is called the "DC bias characteristic" when a DC voltage is applied. Changes in the capacitance (dependent on the DC bias) are rarely seen with a low-dielectric constant MLCC (type 1) but do appear with a high-dielectric constant MLCC (type 2). This is caused by the intrinsic polarization of the ferroelectric (BaTiO3) used by the high-dielectric constant material. For this reason, please consider the dielectric characteristics, the voltage used and the withstanding voltage when making a selection if it is to be used when applying a DC voltage. There is also a tendency for the capacitance to be significantly reduced in miniature-sized capacitors. The DC bias characteristics must also be considered when selecting the capacitance.

PTM פורסם ב: