Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Product List
PDUs Slide 16

Most mission-critical network devices feature redundant power supplies (each with its own power cord) that can connect to separate power sources. However, many other network devices do not have this redundant capability because it has only one power cord. PDUs with ATS provide redundancy for the single-corded devices by allowing it to connect to two separate power sources. Depending on the desired level of power protection, the two sources can be two UPS systems, two generator-supported utility wall outlets or one UPS system and one generator-supported utility wall outlet.

PTM פורסם ב: