Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Product List
PDUs Slide 8

The PDU's digital load meter is perfect for dense network rack environments where managers are trying to get the maximum use out of every device, including the PDU. The PDU's digital load meter allows managers to safely plug in the maximum amount of devices without overloading the PDU. Select models feature two digital load meters. Some models use the two meters to monitor two separate load banks within the same circuit. Other models use the two meters to monitor two separate circuits housed within the same PDU.

PTM פורסם ב: