Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Product List
on off compar
Consideration should be given to how the circuit will operate in “startup” mode, possibly from room temperature or cold-soak conditions, and up to operating temperature. The difference in temperature can be 50 degrees or more in some applications that are mounted in sealed enclosures or cabinets with limited cooling. If the system is microprocessor controlled, consider monitoring temperature in the unit and adjust system timing to allow for variations over temperature.
PTM פורסם ב: