Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Product List
summary
In summary, SSRs use a photo detector to drive an output MOSFET to optically isolate circuits which operate from independent power sources of differing voltage levels. Some of the features and benefits of SSRs include a bidirectional MOSFET which supports both AC and DC switching, no possibility of thermal runaway since there are no bipolar elements, and the ability to switch low to high-voltage signal levels or an AC/DC load current.
PTM פורסם ב: