Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Product List
low cxr
In comparison to the PS7141E-1A device in the previous slide, the chart shown here is from the PS7802-1A low CxR relay data sheet. At 0 V, the typical output capacitance is 11.5 pF, a third lower than the PS7141E-1A vertical Trench MOS device. For the PS7802-1A, the On channel resistance has a typical value of 1.1. Therefore, this device would be better suited for higher frequency applications.
PTM פורסם ב: