Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Product List
t mos
As an example of the effect of the vertical Trench MOS structure, the graph shows the Output Capacitance of a 400 V PS7141E-1A device. Note that the test frequency of this data is at 1 MHz. This device is intended for applications with higher applied voltages. The capacitance value is low when the load voltage on the output is greater than 20 V with a typical output capacitance of about 36 pF at zero volts. This type of device would be appropriate in an AC/DC switching power device or where high-frequency signals above 1 MHz are not primarily passed through this device.
PTM פורסם ב: