Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Product List
chan hor
The SSR structure, shown on the right, has a horizontal structure and provides low channel resistance, with a larger boundary layer, which often contributes to a higher capacitance value. This horizontal structure will tolerate lower voltages than the vertical structure. The material for the horizontal structure can be configured for low capacitance “C” and resistance “R” values, leading to a “CxR” value of capacitance multiplied by resistance. This value of “CxR” is often used as a measure of how the SSR will perform in various applications. Each SSR should be evaluated for performance at the desired frequency of operation prior to its use in the final application.
PTM פורסם ב: