Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Product List
improving transient response
The classical brute-force approach to reducing transient response deviation is to add external capacitance. Unfortunately, this also has the effect of reducing the gain bandwidth. Essentially, adding capacitance provides a greater source of energy for load transients, but also causes the circuit to respond slower and potentially become unstable. This is demonstrated in the red transient deviation. The amplitude is reduced, but at the cost of a slower response with more ringing.
PTM פורסם ב: