Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Product List
ge dpi simple gui2
The DPI GUI allows communication to up to 4 POLs and 2 BUS converters. Enter the trim resistor value in Kohms at the top and select the Trim value in Volts. Then select “Write Settings” for the module to accept the new setting. If this is to become the new permanent setting of the module, select “Store Defaults”. That’s it. The digital trim is capable of 0.4% resolution.
PTM פורסם ב: