Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Product List
tunable loop solution
Tunable Loop is an easy solution that employs two small external components to make the best use of the available capacitance, yielding the lowest transient response. It also helps keep the module stable with increased external capacitance. The RTUNE and CTUNE components are connected in series between the output and the trim pin as illustrated. 
PTM פורסם ב: