Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Product List
input filtering AN04-002 AN04-005
Using the input filter data provided in the datasheet, an appropriate level of ripple can be achieved. As with output ripple, the graphs are based on real measurement data. In this case, the desired target is less than 120 mV peak to peak ripple. Following the graph, users can see that this is achievable with one 22 µF capacitor. The recommendation is to use ceramic caps for best ripple reduction and to use a combination of physically small and larger ceramics to attenuate noise and ripple. The smallest capacitors should be placed very close to the input pads of the module. Application notes AN04-002 and AN04-005 give more details and are available on the OmniOn Power website.
PTM פורסם ב: