Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Product List
four steps to powerup
These simple tools provide a solution with only 4 steps to power up. First is module selection, based on thermal de-rating and operating conditions. The second step is setting up and tuning the output using the voltage programming tool and the tunable loop tool. Next is the input filter selection, based on measured ripple. Last is the selection of any additional digital and auxiliary circuits if needed.
PTM פורסם ב: