Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Product List
Image of ITECH IT8500G+ Series Programmable DC Electronic Load - Battery Drainage

IT8500G+ can perform battery discharge tests in CC mode. When users only need to do battery testing in one or two stop conditions, the other conditions should be set to the specified value (STOP VOLT: 0V; STOP CAP: 999.999AH; STOP TIMER: 99,999s). However, when the test duration meets the STOP TIMER: 99,999s condition, the test will also be terminated. List mode allows users to generate a complex current sequence. Moreover, the mode change can be synchronized with an internal or external signal, to accomplish dynamic and precise testing which can save cost for users. The LIST mode of the IT8500G+ can accurately perform complex arbitrary current change modes at high speeds, and this change mode can be synchronized with internal or external signals to complete precision testing with multiple alignment loads. It can be used in complex applications such as electronic product development, product aging in production lines, and quality inspection.

PTM פורסם ב: