Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Product List
Image of ITECH IT8500G+ Series Programmable DC Electronic Load - I-Monitor

In order to analyze the characteristics of the object to be tested, engineers often need to view the actual voltage and current waveforms with the help of an oscilloscope, where the current waveform needs to be paired with an oscilloscope + expensive current probes, which invariably increases the cost of testing. ITECH’s IT8500G+ features a built-in I-monitor monitoring port, saving the user expensive current probes. They only need to connect the ordinary voltage probe to complete the current waveform monitoring. Using ITECH electronic loads can save users the cost of expensive current probes and monitor the current waveform directly through the I-monitor terminal on the back panel of the load.

PTM פורסם ב: