Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Product List
Image of ITECH IT8500G+ Series Programmable DC Electronic Load - Testing Design Image

IT8500G+ series could also be used for DC/DC module testing. With the advantages of a built-in OCP/OPP testing function, it can monitor the voltage during the test. When the test is completed, the IT8500G+ will automatically present the measured results. If the measured results match the expected value of around 3A, it indicates that the overcurrent protection design value of the DC/DC power module is correct.

PTM פורסם ב: