Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Product List
Image of ITECH IT8500G+ Series Programmable DC Electronic Load - Ripple

Ripple is one of the parameters that must be tested for switching power supplies. Excessive ripple may cause interference to the DUT or shorten the life of the DUT. The IT8500G+ is the load that can complete the traditional configuration of "load + oscilloscope + DVM" to achieve the test project, such as output ripple test, output accuracy test, dynamic response time test, overload capability test, and steady state load performance test.

PTM פורסם ב: