Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Product List
Image of ITECH IT8500G+ Series Programmable DC Electronic Load - Multi-Channel mode

The multi-channel mode of the IT8500G+ is specially designed for optimizing system integration. Through this mode, it can easily build hardware platforms with dozens or even hundreds of channels. It simplifies communication connections. There is no need to purchase expensive communication modules or communication interface expansion cards (such as USB hub, multi-serial card or switch), which greatly saves test costs. For example, IT8500G+ multi-channel mode can greatly reduce the complexity of communication wiring. If controlling 16-channel loads, no need to connect each device to a PC with a LAN cable which will be sixteen cables and a network switch in total. With IT8500G+, only one LAN cable is needed to connect with PC.

PTM פורסם ב: