Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Product List
8BitMCU-Slide5

At a high level, Microchip has four 8-bit architectures which fill a wide range of pricing and performance options: the low-cost and small sized baseline family contains PIC10, some PIC12 and some PIC16 devices; the mid-range family brings optimal cost to performance ratio featuring members of the PIC12 and PIC16 families; the enhanced mid-range family expands on the mid-range devices adding more performance and  memory at a cost-effective price point, and is identified by the one and three subsequent digits following the “F” in the product identification number; and PIC18 devices, featuring the highest performing members in the 8-bit family adding advanced peripherals such as Ethernet, USB, CAN and Real Time Clock Calendar. Microchip’s 8-bit families feature products in a variety of packages with pin counts ranging from six to one hundred pins, providing flexibility to meet most customer design and space requirements.

PTM פורסם ב: