Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Product List
Class D Audio Amplifiers Slide 11
Class D topology utilizes pulse-width modulation (PWM) with a triangle-wave generator. This slide shows a simplified block diagram of a PWM-based, half-bridge, Class D amplifier. It consists of a pulse-width modulator made of a comparator and triangle-wave generator, two output switches (e.g. power MOSFETs), and an external low pass filter to recover the amplified audio signal. The switching frequency for NXP’s Class D amplifiers is typically between 250kHz to 450kHz. The output square wave is pulse-width modulated by the input audio signal, and is accomplished by comparing the input audio signal to an internally generated triangle-wave oscillator. It drives the power output driver switching stage, creating the amplified digital signal before the low pass filter (e.g. Butterworth filter). As shown, this PWM output has a varying duty cycle proportional to the audio signal. After passing through the LPF, the PWM modulated carrier is filtered out and an amplified sinusoidal audio signal drives the speaker.
PTM פורסם ב: