Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Product List
Class D Audio Amplifiers Slide 6
The training module will now shift its focus to the basics of audio amplifiers. Audio amplifier power ratings are determined by a combination of parameters including: the Output Voltage swing (VO); Load resistance (RL); and Package Thermal Resistance (j-a). Using ohm‘s law for power, PO = VO2 / RL, VO increases as Vcc is increased, which yields more output power. When RL and j-a are lowered, PO to the load also increases.
PTM פורסם ב: