Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Product List
Class D Audio Amplifiers Slide 9
The efficiency of an amplifier limits the amount of total power output that is available to drive the speaker or load. A more efficient amplifier runs much cooler, and sometimes does not need a large heatsink or fan for cooling. This slide provides a quick illustration of the wasted power that shows up as heat in the audio amplifier. The gray area is the unproductive power dissipated as heat.
PTM פורסם ב: