Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Product List
Power over Ethernet Slide 10
The other type of power sourcing equipment is the midspan, upon which the remainder of this presentation will focus. A midspan PSE fits in between the switch and the powered device. For example, if a company has a 24-port switch and only five PoE applications, power only needs to be provided on five nodes. This can be a very cost effective solution using single port power injectors on the existing switch. It also provides for an easy upgrade compared to the expense of buying and installing a new switch with PoE.
PTM פורסם ב: