Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Product List
Power over Ethernet Slide 16
PoE is also more reliable in that the power supplies have all of the international safety certifications and power is provided over the CAT5 cabling so there are no hazardous voltages, power overloads, outages, surges or spikes. When PoE is implemented with uninterruptible power supplies (UPS) or battery backups, it allows enterprises to distribute power, even when the AC electrical power is down.
PTM פורסם ב: