Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Product List
Power over Ethernet Slide 27
If the design is currently 100 Base-T, or 100 megabits/sec of information, will migrate to 1000Base-T, or a gigabit/sec in the future? If the answer is yes, recommending a gigabit solution is the best because the higher data rate will be there when the move is made. Meanwhile, it is backward compatible to support current applications.
PTM פורסם ב: