Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Product List
Power over Ethernet Slide 9
The IEEE 802.3af standard defines two different types of PSEs: endspan and midspan. An endspan PSE integrates the power sourcing functionality with a network switch. This device can be 8-port, 12-port, 24-port or more with the capability of delivering power on any one or all of those ports. One of the disadvantages is the majority of the installed switches in existing networks still are not 802.3af compliant so there is no protection against equipment damage.
PTM פורסם ב: