Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Product List
Power over Ethernet Slide 13
One advantage of PoE is that the power supply can be located anywhere within 100 meters of the application versus a separate power source that would need to be located within 6 feet. With PoE, the power supply can be located in a wiring closet or anywhere that is away from the application. So power and data are united with only one wire, versus two wiring solutions. This results in lower installation costs since PoE eliminates the need for running both data and power wires to each network device.
PTM פורסם ב: