Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Product List
Power over Ethernet Slide 6
There are two basic components in an IEEE 802.3af compliant PoE network: 1) Power Sourcing Equipment (PSE) supplies the power and then a Powered Device (PD) receives and utilizes the power. When the PSE connects to a network device, the PSE determines or “discovers” if the device is a PD or not. This prevents non-PoE enabled Ethernet equipment from receiving power, which could cause damage.
PTM פורסם ב: