Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Product List
powerSPIN Motor Control ICs Slide 17

The L6206 and L6226 devices integrate all the features of the previous two ICs, as well as providing the possibility of adjusting the maximum current protection through a resistor connected to a dedicated pin. It is also possible to use this protection feature to implement a PWM current control. So one can see from the L6205 to the L6206 and L6226 there is an increase in complexity.

PTM פורסם ב: